Printing Graphics
You print a graphic, for example, to present it to a customer or to get an overview.
To print a graphic:
- In Graphics Editor, on the File menu, select Print, and then click Print.
- In the Print dialog box, select the printer you want to use and set other print options.
- Click Print.
You can set up a page for printing to print a graphic in a specified way.
To set up a page for printing:
- In Graphics Editor, on the File menu, select Print, and then click Page settings.
- In the Page Setup dialog box, enter paper size, orientation, margins and other properties.
NOTE: The print settings apply for all printouts until you change them.
You can preview a print to make sure the printed page will turn out the way you intended.
To preview a print:
- In Graphics Editor, on the File menu, point to Print, and then click Print preview.
- In the Print preview dialog box, set the number of pages you want the graphic to print on.
- Click Close.